2/17/2012 8:42 AM | |
Joined: 10/10/2005 Last visit: 6/15/2023 Posts: 1909 Rating:
|
Hello, in TIA Portal you will find the instuctions for each modul. Generate a new block (example FC) and insert per Drag&Drop a timer (example "S_IMPULS") from the Basic instruction in the program editor. Mark with the coursor this modul and use the "F1"-bottom. So you will see the online help for programming and assign the parameters for this timer. Please find also an example in the internet: http://support.automation.siemens.com/WW/view/de/39309294 With best regards |
3/1/2012 10:04 AM | |
Joined: 10/10/2005 Last visit: 6/15/2023 Posts: 1909 Rating:
|
Hello, consider, the TIA Portal has an other philosophy character as the STEP 7 V5.x and the S7-200 system. But the programming methode in TIA Portal is the same as by the conventional STEP 7 tools. If you have programmed STEP 7 projects, you can also migrate these projects in the TIA Portal. See in this case the FAQs in the internet: http://support.automation.siemens.com/WW/view/de/56314851 http://support.automation.siemens.com/WW/view/de/54173102 With best regards |
Follow us on