6/14/2010 8:48 AM | |
Joined: 9/5/2007 Last visit: 12/9/2024 Posts: 24 Rating: (0) |
Hello Siwarexi, I have a siwarex module 7MH4950-2AA01 and the LC (i.e. connected with 6-wire system) which we are using with a characteristic value of 2 mV/V.So the measurement signalshould be in the range of (2 mV/V x 6 V) = 0 ... 12 mV.
Regards, DESH. Splitted from Excitation voltage. |
Last edited by: O_Moderator at: 6/14/2010 12:06 PMnew subjectt after splitting Last edited by: DESH at: 6/14/2010 8:49 AM |
|
Follow us on