3/6/2017 11:49 AM | |
Posts: 6 Rating:
|
Hi all, I've got a problem with the adding of one CP343-1 Lean to an S7 300 CPU (6ES7 314-1AG14-0AB0). when I put the CP on the rack, there is a fault of the CPU, is normal.. I modify the configuration to add the CP and one correct IP address connected to the PN network ... all is OK but when I want to transfer the configuration into the CPU through the MPI bus (with my PG) TIA PORTAL give me an error (MPI address 3 unreachable) and after looking the HW the third MPI address is the CP... So the configuration still in fault and the CPU too... I've never seen that before. Have you any ideas ? Thanks all ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/6/2017 3:43:07 PMNew subject after splitting |
|
3/7/2017 5:51 PM | |
Posts: 6 Rating:
|
|
3/7/2017 5:52 PM | |
Posts: 6 Rating:
|
|
3/8/2017 12:22 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, the easiest is to load the CP over Ethernet. Have a try! regards, |
FCK WAR! |
|
Follow us on