10/4/2018 5:22 PM | |
Posts: 2 Rating:
|
Arash Noori Gold target Hi Dear friend I have a problem ..... The full profile of the project is as follows and project Run inPCS7: "PLC S7- CPU 315 - 2DP" "Monitoring PC" "Modbus RTU" "CP-343 (On the plc side)" "I.E. General (On the pc side)" As you see in the photoTheIP address is identical in "Simatic manager" and "WinCC" and Before downloading the program via ethernet(cp-3434), I first downloaded "HW config settings" to CPU with Pc Adaptor, Which allows the CPU to recognize the network card, And then download the program to CPU and run but the link between WinCC and CPU is not connected. Even the connection between the tags is established AND when I choose a tag with Flag it's WORK ....look at the Picture! In other words, the problem is that when I run the project, connection icon color marked in the photo does not turn to green. please tell me where is my mistake? Attachmentfinal.pdf (57 Downloads) |
10/4/2018 11:06 PM | |
Posts: 2 Rating:
|
Can give a clearer amount .... Which part of the settings is wrong |
Follow us on