7/22/2015 6:01 PM | |
Posts: 160 Rating:
|
Hi, please take a look at this thread: Regards, Janko |
This contribution was helpful to
1 thankful Users |
7/23/2015 10:05 PM | |
Posts: 4 Rating:
|
I could solve the problem of the cámera, I installed a incorrect GSD of cognex, now the problem i have is the same that you post me, but i have a question. You say some about the the Slots, do you refer this?? (photo) I'm starting learning in TIA Attachmenterror.docx (735 Downloads) |
7/24/2015 9:44 AM | |
Posts: 160 Rating:
|
Hi, Could you send us a picture of your second picture again but selecting "Bufer de diagnostico" insted of "Estado de diagnostico" because SF led error is a bit vague... Anyway, the answer on your question is NO. By slots I meant (see photos in attachments)... If you are able to send us a whole project (for me I'll have to save it as TIA Portal V12 file, cause I do not have V13), please do it! Regards, Janko PS: You do not have to explain your self, saying that you are learning TIA AttachmentPhoto 1 2.DOCX (712 Downloads) |
Last edited by: jankoslayer at: 7/24/2015 9:46:40 AM |
|
7/25/2015 12:30 PM | |
Posts: 160 Rating:
|
Hi, can you confirm that all data packets introduced in various slots (0:58) of your video Profinet problem perfectly correspond to the one you configure in software where you actually configure Cognex 5100 Profinet interface... So I imagine that you have a software for configuring Cognex... I also presume there's a possibility to introduce various data packets in various slots (I am not talking about TIA anymore, I am talking about Cognex software for configuring data packets for profinet interface). Janko |
7/25/2015 12:33 PM | |
Posts: 160 Rating:
|
Send us also a photo where you configure your Cognex in whatever third party sw for Cognex Profinet configuration... Janko |
3/10/2016 4:40 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating:
|
New question published by lianndt is split to a separate thread with the subject Define the I/O slots of Cognex in TIA V13. Best regards |
Follow us on