9/18/2018 11:13 AM | |
Posts: 9 Rating: (0) |
Hello all, i have a problem on configuring my sensor PT100 to Sirec D300, i have installed based on this manual SIREC D200/D300/D400 Display RecordersBut the chart remain above 100%. did i miss something ? i use pt100 2 wire and connected like the manual. does need anymore setting on the scaling, logging methods, etc ? bellow i attach picture of the analog input i use. Best Regards, Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/18/2018 2:42:28 PMNew subject after splitting Last edited by: Jen_Moderator at: 9/18/2018 2:43:03 PMOptimized link. |
|
10/2/2018 4:25 AM | |
Posts: 9 Rating: (0) |
Dear danw, Thanks for the guide. I have 1 channel died. Im following your step in different channel and it work. Best Regards, Teddy |
Follow us on