Industry Online Support
Technical Forum
1/21/2008 2:23 PM | |
Joined: 9/29/2005 Last visit: 4/26/2022 Posts: 313 Rating: (24)
|
Hi Tommy! general information you will find here: http://support.automation.siemens.com/WW/view/en/22253483 (dedicated to your case: Page 4-3) I think the Pins on Sitrans P side you need are: +Uo, -Ub, +Ub , Voltage out, 0V, 24V. Maybe you mixed up voltage output and current output by connecting to S7-200 voltage input? Do you have the possibilty to measure with a voltmeter what "+Uo" provides when 0,0V expected? regards Lifrasil |
2/1/2008 1:41 PM | |
Posts: 4 Rating: (0) |
Hi Lifrasil I have connected the same preasure transmitter (SITRANS P serie Z) on Analog I/O EM 235 and I had 0,0V on Analog input!!! (After thatI have connected SITRANS P serie Z , with output signal 4-20mA to CPU224xp ( like this way http://support.automation.siemens.com/WW/view/en/25204813) and itwas O.K.) Best regards, Tommy |
Follow us on