6/6/2020 6:00 AM | |
Joined: 4/14/2017 Last visit: 10/23/2022 Posts: 2 Rating:
|
THANK YOU VERY MACH !!!! |
6/6/2020 9:26 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating:
|
I haven''t used that CPU and I will answer in general. Frequency is measured in Hz that is how many pulses per second and if the encoder is not moving and the inputs are not receiving any pulses then the frequency is zero pulses per second or 0Hz. Period is 1/frequency and if the frequency is 0Hz then the period is 1/0 which is invalid and according to the manual it should read 25s until measured value is available. Velocity is about the same and depends on the frequency and the time base. Have a look at this manual. |
Follow us on