7/17/2015 11:24 PM | |
Posts: 2 Rating:
|
Hello, I have a device which I want to control using modbus communication. I use the S7-1200 CPU 1214C (6ES7214-1HG31-0XB0) witch Tia Portal V12 I can read some parameters but I have a problem witch some registers with offset from 12288. I use the MB_Client block. The modbus function 4 for parametr MB_DATA_ADDR have range 30001 do 39999 so the parameter MB_DATA_ADDR= 42291 (30001+12290). But it is out of range. And this is not work. In attachment there is description of the communication. Attachmentmodbus.pdf (120 Downloads) |
Follow us on