9/28/2017 1:47 PM | |
Joined: 4/28/2017 Last visit: 12/6/2024 Posts: 149 Rating:
|
Dear Experts, Pleasant Evening to all, I Made A Program To Establish Modbus TCP/IP Communication Between the below PLC's. I Used "S7-1511-1 PN" as Client, And, "S7-1212C DC/DC/DC" as Server. There are no Errors in the Program. Compiling and downloading made successfully. But, During Online state, I Turned On the "START" Boolean bit in "MB_CLIENT" block. It shows same FALSE status in the BUSY and DONE Bit output. And, Then Periodically I can see this Error Code (16# 80C6) in Status Node. I think the Server isn't Responding. Could you please anybody help me with this. I have attached my Program and Screenshots. AttachmentModbus_TCP_2807.zip (313 Downloads) |
Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
9/28/2017 1:48 PM | |
Joined: 4/28/2017 Last visit: 12/6/2024 Posts: 149 Rating:
|
Here You Can have my sample Screenshots. AttachmentMOdbus_TCP.zip (427 Downloads) |
Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
Follow us on