8/3/2012 11:04 AM | |
Joined: 3/21/2006 Last visit: 2/10/2025 Posts: 10239 Rating:
|
|
8/3/2012 11:53 AM | |
Posts: 71 Rating:
|
I don't get that question, I can only choose "Ok" and nothing happens then. I have attached a picture on the window that appears. |
8/3/2012 12:09 PM | |
Posts: 71 Rating:
|
Now I have run a OS Update without the factory reset setting. Same problem, it feels like I can't do anything more, the panel is maybe broken? |
8/3/2012 1:14 PM | |
Posts: 3037 Rating:
|
Hello bowler, You can see the right image to the WinCC flexible version in the attachment in the following link. What connections are there between the version designations in WinCC flexible? Tweety |
8/7/2012 8:48 AM | |
Posts: 71 Rating:
|
I want to the BIOS in MP370, is it possible? Normally on a PC it says for example "Press F2 to setup", but in MP370 there is no message during start up. |
Follow us on