4/2/2012 2:12 PM | |
Posts: 8946 Rating:
|
You select correct adress? You enbable the MPI channel on TP? |
4/3/2012 2:16 PM | |
Posts: 3037 Rating:
|
Hello, You can find more about download a project via MPI in the next link. How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Which adapter do you use? PC/MPI-Adapter and USB/MPI-Adapter are not released for transfer. You can see this in the following FAQ attachment 1. What transfer options are available in the various operator panels? Tweety |
Follow us on