4/2/2012 7:37 AM | |
Posts: 12 Rating:
|
Dear expert, I have problem with my touchpanel model TP177A.......i can't download ng program from wincc flexible...thanks good day........ |
Last edited by: O_Moderator at: 4/2/2012 11:31 AMnew subject after splitting from /tf/WW/en/Posts/71595#top |
|
4/2/2012 7:45 AM | |
Joined: 4/22/2010 Last visit: 2/26/2025 Posts: 5697 Rating:
|
Hello, Please tell us a bit more like settings, used cable, etc. Regards, Marcjan |
Problem solved? |
|
4/2/2012 1:32 PM | |
Posts: 12 Rating:
|
Hello Marcjan, I used MPI cable connected to HW adapter going to the PC....Now the problem is i can't download program to the simatic panel.....the error display shows that "it can't establish due to cable etc."....We use wincc flexible 2007....We go to siemens Jeddah just to testing the simatic panel and the cable we used and they tell it's working....Now i don't know the problem....can anyone help me.... |
Last edited by: darkknife at: 4/2/2012 1:41 PMLast edited by: darkknife at: 4/2/2012 1:40 PM |
|
4/2/2012 2:08 PM | |
Joined: 4/22/2010 Last visit: 2/26/2025 Posts: 5697 Rating:
|
Hello, Check the tranfersettings in your panel, see [url=http://support.automation.siemens.com/WW/view/en/21084461] manual[/url] chapter 6.1. Then check settings off Pc/PG interface, baudrate should be the same. Then check settings in wincc, adress of hmi should be the same. Regards, Marcjan |
Last edited by: Marcjan at: 4/2/2012 2:17 PMProblem solved? |
|
4/2/2012 2:12 PM | |
Posts: 8946 Rating:
|
You select correct adress? You enbable the MPI channel on TP? |
4/3/2012 7:31 AM | |
Posts: 12 Rating:
|
Hello, Still i can't transfer.....i follow step by step procedure in the manual that you give it to me....somebody telling i need a software....is that possible that software is my problem.....i only have 1 day to finish this.....tomorrow my boss is coming pls help me...thanks in advance |
4/3/2012 2:16 PM | |
Posts: 3037 Rating:
|
Hello, You can find more about download a project via MPI in the next link. How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Which adapter do you use? PC/MPI-Adapter and USB/MPI-Adapter are not released for transfer. You can see this in the following FAQ attachment 1. What transfer options are available in the various operator panels? Tweety |
4/7/2012 9:31 AM | |
Posts: 12 Rating:
|
thank you very much tweety and experts.....i hope i can solve the problems in communicating simatic panel to pc.... |
This contribution was helpful to
1 thankful Users |
Follow us on