7/17/2012 5:42 AM | |
Joined: 3/21/2006 Last visit: 3/17/2025 Posts: 10239 Rating:
|
Hello, Try it with"Reset to factory settings" option fromhttp://support.automation.siemens.com/WW/view/en/26437978 Best regards, Hristo Mihalev
|
7/17/2012 10:57 PM | |
Posts: 3 Rating:
|
Hi Umencho, I try all reset with a MPI/USB cable and dont work. I need the RS232/PPI cable? |
7/18/2012 10:57 AM | |
Posts: 3037 Rating:
|
Hello, Yes, do you need a RS232/PPI multi-master cable or USB/PPI cablefor the reset. You can find these cable in the following FAQ. What transfer options are available in the various operator panels? Tweety |
7/19/2012 10:54 AM | |
Posts: 3037 Rating:
|
Hello eligodoy, You need this cable RS232/PPI 6ES7 901-3CB30-0XA0 for Operating system update with Reset to factory settings. The procedure of this is described in the following FAQ. http://support.automation.siemens.com/WW/view/en/26437978 Tweety |
11/6/2012 11:10 AM | |
Posts: 3037 Rating:
|
Hello Eli Godoy, You do not use any USB adapter for the transfer to OP177B. Using USB RS232 adapters and USB Ethernet adapters When using the RS232/PPI Multi-Master cable, zero modem cable or Ethernet connections, you can only use the "real" interfaces for project transfer. "Real" interfaces are interfaces without implementation via USB. This means that you cannot use any "USB to serial" or "USB to Ethernet" adapters. See the following link. What transfer options are available in the various operator panels? If you are using high bit rates, then you must implement the RS232/PPI multimaster cable with "E-Stand 03" (development status 03) or higher. You see in the following link, which settings do you need with RS232/PPI multimaster cable. see the point 4 --> 1.2 How do you do an operating system update (OS update) on operator panels? Tweety |
Follow us on