1/29/2014 3:23 PM | |
Posts: 1299 Rating: (135)
|
Hello, thereis a lot of information in manual of wincc v12 K!ke |
Last edited by: K!ke at: 1/29/2014 3:23 PM |
|
1/31/2014 3:06 AM | |
Posts: 10 Rating: (0) |
Thanks again for your reply, As for configuration, there was very little for OPC UAin theruntime settings (it can't even be disabled), but I enabled no security for testing. After starting the runtime, when I check for any available servers using a discovery client, nothing appears. Also, the connection is refused when trying to connect manually using the port number configured in runtime settings. I then found this document: Communication via OPC UA in Conjunction with a SIMATIC HMI Comfort Panel In section 5 it has notes on installing WinCC Runtime Professional V11 SP2 with OPC, showing under tools the option of installing all the different OPC servers, and also showing what services to check for a successful OPC installation. I decided to try andreinstall our old copy of WinCC Professional V11 SP2, and still did not see these options. The major distinction is that I guess I'm only installing the engineering environment, not the "Runtime". I assume there is a separate installation media for WinCC Professional vs. WinCC Runtime Professional just as there are two separate licenses? If this is the case, I do not have the Runtime installation media, and will have to discuss this with our distributor. |
Last edited by: CS Moderator at: 1/31/2014 2:52 PMLink replaced by a permanent one Last edited by: mCarlson at: 1/31/2014 3:14 AM |
|
12/4/2014 2:24 AM | |
Joined: 12/17/2011 Last visit: 4/27/2024 Posts: 4 Rating: (1) |
Hello, mCarlson: I meet the same problem. Have you already solved the problems? Solutions? Thanks tbkh |