9/25/2019 1:02 PM | |
Posts: 2 Rating:
|
Hi all, I have problem with PID_Compact block. Input to block from DB is not changing, but PID_Compact.Input on trace is going to zero. Input to block later on is changed because PID output is changing and it's really slowing down. So my problem is why PID_Compact.Input is going to zero and from where if value which I'm sending to PID_compact.Input is not zero. I have recorded mode, state, warning and error of PID controler and there is no any change during this behavior. Also time of zero input is 100 ms. Picture of trace in attachment. Thank you in advance ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/25/2019 15:10:36New subject after splitting |
|
Follow us on