4/21/2013 11:46 AM | |
Posts: 70 Rating:
|
Hello, I have a problem with positioning S110, so I would like to sincerely ask for advice. Procedure: First, I crossed the configuration starters to the drive, then I recorded program (see Pictures.zip) of the TIA Portal V11 to the PLC. In the first I said inverter to run (ONOFF1 = 1), then I activated the input EPOS_jog_2 = 1, the start-up balls on inductive switch, I activated the input IS3 (1.zprava) = 1 and I finally activated the input EPOS_positioning_Start = 1 (see Setting homing.JPG). Activating one of the inputs of the color sensor (see Position.JPG) but not to move to the position (output Actual_position block ST111 was worth about 400,000). How should I achieve that after striking the inductive switch (IS3 (1.zprava) = 1), the value of Actual_position = 0? Thank you in advance for your reply
AttachmentPictures.zip (64 Downloads) |
5/14/2013 7:20 PM | |
Posts: 70 Rating:
|
Hi, Now we have a problem with starters here: /tf/WW/en/Posts/91636#top |
5/16/2013 4:52 PM | |
Posts: 70 Rating:
|
Ok |
Follow us on