3/4/2010 9:38 AM | |
Posts: 13 Rating:
|
Hello, I have configured a CM1241 RS232 card to send and receive characters to/from Hyper Terminal. I have used a very simple program which consists of two blocks (PtP_SEND & PtP_RECEIVE). No Special logic. Every time i try to enter chars from HT, i notice a strange problem. In the buffer area of the block PtP_RECEIVE i lose the first two characters of each string i enter through HT. For example : "Hello", i see only"llo" or "George" , "orge". I have tested any method for receive characters end (message timeout, characters sequence e.t.c.). I have attached my program. Can you please advice anything ? Thank you very much. Regards, George AttachmentSMS_ALSOS.zip (122 Downloads) |
3/9/2010 8:25 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already discussed in the following thread Exchange data via RS232 and Hyper terminal with S7-1200. Best regards O_Moderator |
Follow us on