9/18/2016 9:26 PM | |
Posts: 5225 Rating:
|
Welcome with your first post. From your description it is not possible to determine the origin of the problem. Devices do only what we (operators / programmers) command them to do. Think about what auxiliary program you can write to help you diagnose the program. For example... let us say you have 3 sources that can start the system. Add a counter for each start trigger. So you will have 3 counters that keeps track of how many times the system is started. When the scheduled stop occurs, you can reset all the counters. Now at least you have a record of where the start originated from. Considering that I do not know your system, my suggestion will not work. But think of things like this to assist you to pin down the origin of the issue. Good luck in finding the Gremlin. |
This contribution was helpful to
1 thankful Users |
9/19/2016 8:36 AM | |
Joined: 7/9/2013 Last visit: 9/18/2019 Posts: 3 Rating:
|
How can I check this Switch? What does it mean? |
9/27/2016 12:26 PM | |
Posts: 42 Rating:
|
Hi, can you control that the output for your machine is present in only a segment in PLC?!?
|
Follow us on