6/27/2023 10:06 AM | |
Joined: 10/8/2018 Last visit: 9/5/2023 Posts: 9 Rating:
|
Hello everyone, We have a problem with the U/E module on a 4-axis CNC machine consisting of the following hardware configuration: - Siemens 6FC5210-0DF22-2AA0 Sinumerik PCU 1.2GHz, 256RAM - Siemens 6SN1146-1AB00-0BA1 Simodrive U/E module int-ext.5/10KW (VERSION A) - Siemens 6FC5447-0AA00-0AA1 LT-MODUL - Siemens 6FC5410-0AY03-1AA0 Sinumerik 810D CCU3.4 software vers. 6.5 From the pictures in the attachment, you can see that the red 3rd LED is lit, and in the manual I found that it indicates that there is a problem with the power supply. I checked the voltage at the input and it is 407V, while the voltage on the DC bus is around 590V (after I give permission from the auxiliary circuit). Thanks in advance!
Attachmentsimo1.pptx (67 Downloads) |
Follow us on