10/9/2021 2:23 AM | |
Joined: 4/25/2019 Last visit: 10/6/2022 Posts: 6 Rating: (0) |
Добрый вечер коллеги. У меня такая же проблема с интеграцией RED670, REB500 в SicamPas 8.14. Когда я выгружаю scd-файл подстанции из PCM600_2.10 и загружаю его в SicamPas 8.14, я получаю следующие ошибки: "Starting the error report for 1.IED...;10/8/2021;4:28:58 PM; The validation of IED 'SEA2TCPMRED1' (device type: 'IED670' from manufacturer: 'ABB') is finished with errors.;10/8/2021;4:28:58 PM; Contact your 'ABB' support to solve the problem..; Error at line 897, char 8 --> '<ReportControl name="rcbStatUrg" desc="PCM600 auto-generated RCB" datSet="StatUrg" confRev="500" intgPd="3000" bufTime="100" buffered="true">';10/8/2021;4:28:58 PM; ('Message: The required attribute 'rptID' is missing.'); Error at line 904, char 8 --> '<ReportControl name="rcbStatNrml" desc="PCM600 auto-generated RCB" datSet="StatNrml" confRev="400" intgPd="3000" bufTime="100" buffered="true">';10/8/2021;4:28:58 PM; ('Message: The required attribute 'rptID' is missing.'); Error at line 911, char 8 --> '<ReportControl name="rcbMeasFlt" desc="PCM600 auto-generated RCB" datSet="MeasFlt" confRev="300" intgPd="3000" bufTime="100">';10/8/2021;4:28:59 PM; ('Message: The required attribute 'rptID' is missing.'); Ending the error report for 1.IED.;10/8/2021;4:28:59 PM;" What can you advise to solve this problem? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/11/2021 10:34:55New subject after splitting |
|
Follow us on