Industry Online Support
Technical Forum
11/7/2007 4:58 PM | |
Posts: 145 Rating: (3) |
Hi, |
11/9/2007 2:45 PM | |
Posts: 1776 Rating: (95)
|
Hi, see FAQs http://support.automation.siemens.com/WW/view/en/21954452 http://support.automation.siemens.com/WW/view/en/25554088 April |
11/12/2007 12:14 PM | |
Posts: 1275 Rating: (123)
|
Hi Nikola, The easiest way to set this filter manually is in runtime, using the alarm control object's toolbar (in v6.0 it's the third icon from left to right, the selection dialog button). You can select a time window, so all alarms in that period will be displayed. The filter can be made dynamic by using the alarm control object's "MsgFilterSQL" property. Filtering will help you diagnose your problem... Regarding the "segment" issue, you can get some info here. With ttaht you can see you must configure the single segment settings. While defining archive settings, take a look at this FAQ, regarding their effects on the system performance. Best regards, Danielle |
Last edited by: Danielle at: 12.11.2007 12:17 |
|
11/13/2007 1:34 PM | |
Posts: 6 Rating: (0) |
Thanks ppl for help... it helped me much... Best regards... Nikola |
Follow us on