7/12/2009 6:41 PM | |
Joined: 5/28/2008 Last visit: 5/11/2024 Posts: 4506 Rating: (836) |
Hello tyura, The TP177 micro may need to recalibrate. Follw the folloing procedure: Power up the screen and go to control panel. Select OP, Touch, Recalibrate. And then follow the instructions and tell us if your problem has been solved. Regards, |
Ayman Elotaify |
|
10/1/2009 8:28 PM | |
Posts: 3 Rating: (0) |
I think this may be an inherent issue with the TP177micro. I have 2 customers who have had buttons that are set/reset bit used as a momentary pushbutton that fail to reset. This has caused overtravel problems on numerous occasions on many machines. We are currently looking at moving to a TP177A since we haven't had this problem. Also, we have tested this with two TP177micro panels, one that had the problem in the field continued to fail and the other worked fine. |