7/15/2014 9:52 AM | |
Joined: 10/28/2008 Last visit: 7/21/2023 Posts: 245 Rating:
|
Hi all. I would like to ask you for support with diagnostic repeater (6ES7 972-0AB01-0XA0). It works nice with DR-CfgData module inserted in repeater in HW configuration (please see attached pictures "TopologyDisplayOK.jpg" and "HwConfigOK.jpg"). But I have a problem withTSYNC-Diag-Module inserted in HW configuration. (See pictures "HwConfigNotOk.jpg" and "ProfiTraceRepeaterFlt.jpg"). Maybe I know where is a problem but I am not sure. There are information in documentation (Diagnose_Repeater_e.pdf): in chapter 6.2.2: Configuring the monitoring functions for the clocked PROFIBUS bus system (see picture "ConfigureTSYNC.jpg"). Point is that I think I have to set clocked Profibus bus system. But I am not able to find "Clocked interrupts" in CPU settings. I cannot find the "Select DP Master system used" etc... My CPU: CPU414-4 H (6ES7 414-4HM14-0AB0, V4.5). If you have any experiences with these settings please let me know! Thank you in advance ! Georgio
AttachmentDiagnosticRepeater.zip (147 Downloads) |
Georgio |
|
7/16/2014 11:03 AM | |
Posts: 1368 Rating:
|
Hello, i am sorry, but thePLC must support this (isochronious mode). And yourPLC does not http://support.automation.siemens.com/WW/view/en/15218045 You can use the following S7-400 PLCs S7-400 CPU Standard CPU 412-1 ab V3.1 6ES7 412-1XF03-0AB0 S7-400 CPU Standard CPU 412-2 DP ab V3.1 6ES7 412-2XG00-0AB0 S7-400 CPU Standard CPU 414-2 DP ab V3.1 6ES7 414-2XG03-0AB0 S7-400 CPU Standard CPU 414-3 DP ab V3.1 6ES7 414-3XJ00-0AB0 S7-400 CPU Standard CPU 416-2 DP ab V3.1 6ES7 416-2XK02-0AB0 S7-400 CPU Standard CPU 416-3 DP ab V3.1 6ES7 416-3XL00-0AB0 S7-400 CPU Failsafe CPU 416F-2 ab V3.1 6ES7 416-2FK02-0AB0 S7-400 CPU Standard CPU 417-4 ab V3.1 6ES7 417-4XL00-0AB0 |
Last edited by: Pittiplatsch at: 7/16/2014 1:32 PM |
|
7/17/2014 8:02 AM | |
Joined: 10/28/2008 Last visit: 7/21/2023 Posts: 245 Rating:
|
HelloPittiplatsch. Thank you for your answer. I am surprised that my CPU does not support isochrone mode OK, I will try it with CPU which supports isochrone mode. Thanks. Georgio |
Georgio |
|
7/17/2014 8:17 AM | |
Joined: 10/28/2008 Last visit: 7/21/2023 Posts: 245 Rating:
|
Helloeisenpferdreiter. I am sorry I think I do not understand your comment properly. I think that if I use any module from list of the slave it should work. PLC (Master) sends confuguration data to the slave (repeater), slave should accept these data and answers. But asPittiplatschasnwered that I have PLC with no support to isochronne mode, so I suppose that the configuration data sent to slave are not consistent and therefore there is configuration mismatch... Georgio.
|
Georgio |
|
Follow us on