5/14/2019 8:58 AM | |
Posts: 6 Rating:
|
Bonjour Je rencontre un problème avec un adaptateur port série / USB, je n'arrive pas à établir une connexion MPI avec une CPU 315-2DP. J'ai vérifié au multimètre mes broches du câble côté port série et ni le pin 2 ou le 7 me donne le 24V .. J'ai configuré la connexion et le câble à la même vitesse de connexion (19,2 kbit / s). Mais j'ai toujours le message d'erreur 256: 1021. Merci d'avance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/14/2019 09:57:43New subject after splitting |
|
5/14/2019 3:12 PM | |
Joined: 9/27/2006 Last visit: 3/14/2025 Posts: 12344 Rating:
|
Translation from the French text:
Hello AssystemLEGAL; Do you have access to the PC Adapter USB manual? Have you looked up the PG/PC interface setup required for this adapter, or checked the active LEDs on the housing, this is important information you can find here: PC Adapter USB manual : https://support.industry.siemens.com/cs/ww/en/view/16983464 Note that the manual, as with most Siemens documentation, can be downloaded in many languages (French is available for this one); check the Language link in the download page. The active LEDs will tell you is the CPU is providing power to the adapter and if there is a communication connection established between the USB port and the CPU. The PG/PC interface will set the comm parameters for the adapter to connect to a MPI or Profibus port on the CPU. Provide us with more information on the adapter results once you check this information and we may help you better. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 05/14/2019 15:22:42 |
|
5/14/2019 3:26 PM | |
Posts: 6 Rating:
|
Sorry I forgot. I use a virtual XP to use Step 7 Lite with VMware. My adapter Serie Port/USB is install to the VM and configurate Thanks |
5/14/2019 3:48 PM | |
Joined: 5/12/2006 Last visit: 3/14/2025 Posts: 22588 Rating:
|
and which USB/RS232 adapter you use? |
5/14/2019 3:52 PM | |
Posts: 6 Rating:
|
An adapter USB 2.0 (type A) to serial RS 232 converter by goobay compatible to siemens |
Follow us on