Industry Online Support
Technical Forum
7/25/2007 8:33 AM | |
Posts: 3149 Rating:
|
Hi which WinCC version are you using? Could you please attach your logfiles from folder ..\wincc\diagnose here in the forum? nemo |
7/27/2007 7:03 AM | |
Posts: 45 Rating:
|
hi, im using wincc v6 sp3 and here are the log files.. thanks Attachmentwincc diagnose.zip (35 Downloads) |
7/27/2007 2:05 PM | |
Posts: 1275 Rating:
|
Hi Azrael, There are some erros in your logs, like: //==================================================================== // WinCC reported exception with code: C0000005 ACCESS_VIOLATION // Date: 19.07.2007 - Time: 05:31:48 // Caused at logical address 00429ADA 01:00028ADA This means the script engine has crashed. 255,22.07.2007,15:21:44:000,1007001,4,,PETRON_SERVER,SCRIPT,ExecuteError in Action @3 255,22.07.2007,23:55:01:984,0,4,,PETRON_SERVER,ArchiveManager,Failed to switch archive(Type:1):PETRON_SERVER_PETRON#HMI#22_ALG_200707221601 ! Check this out. You should clear those errors... try running your system unde APDIAG, it should help checking for scripting errors.. Best regards, Danielle |
Follow us on