12/17/2015 6:41 AM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating: (3006) |
Hi, there is no HSP for this Version of the CP available. From the delivery Notes you can project the V1.2 and use it with the CP V1.3 without problems Firmware version V1.3.3 succeeds version V1.2.3 and contains product improvements. With the update, the CP 343-1 (order no. 6GK7343-1EX21-0XE0) is functionally compatible with the predecessor version. It can therefore be configured with the same STEP 7 / NCM version. If you use only the compatible functions, it is not necessary to upgrade STEP7 or NCM. https://support.industry.siemens.com/cs/ww/en/view/35681318 Regards Christoph |
This contribution was helpful to1 thankful Users |
4/9/2018 12:04 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (171) |
New question published by Markstronic is split to a separate thread with the subject Kindly advice is there change made on new version iIP627C6EQ2020-0AC03-5XX0. Best regards |
Follow us on