12/2/2015 12:57 PM | |
Posts: 29 Rating:
|
Hello, I am having an issue while using virtual machines (tried both with VirtualBox and VMWare) and connecting to a S7-413-2DP controller using a PC Adapter v5.1 connected to my PC via serial port. When I go to Set PG/PC Interface and select the MPI interface(or Auto) I have no Local Connection tab there.On this tab I can choose whether I'm using COM or USB port. It seems that when it is not available it cannot connect trough the COM port.
(opens in a new window) On a Virtual Machine (VirtlaBox, VMWare) with the option missing. When that option is not available, I cannot connect to the PLC, neither view accessible nodes. Does anyone have any ideas on what causes this problem and how can be resolved? Thanks in advance! |
Last edited by: Arucad at: 12/2/2015 12:59:21 PMLast edited by: Arucad at: 12/2/2015 12:59:48 PMEdited typos |
|
12/2/2015 1:59 PM | |
Posts: 29 Rating:
|
I am having some trouble when trying to add the host com port to the guest machine. I will come back here, when I've done it. |
Follow us on