6/14/2007 10:28 PM | |
Posts: 3 Rating:
|
I've just tried to install WinCC version 6.2 (incl. SQL Server 2005 SP1) and I'm experiencing problems with the Graphics Designer. When I try to open Graphics Designer, I get the error message "Fatal error! Failed to create APC host! Terminating!". When I select "OK" to this message, I get 4 subsequent error messages (screen dumps of all messages attached). I've tried the installation on two different pc's running Windows XP SP2 and Windows 2000 Pro SP4 respectively, but with the same result. Has anyone seen this issue before and if so, what is the solution? Thank you in advance Thomas Sörensen AttachmentWinCC error messages.zip (181 Downloads) |
Follow us on