Industry Online Support
Technical Forum
5/28/2007 12:13 PM | |
Joined: 10/18/2006 Last visit: 7/29/2024 Posts: 163 Rating: (3) |
Hi folks ! I´ve got two questions related to PCS7 OS (with version 6.1 SP1) and these are: - In the attached .pdl file you can see there are several buttons. Let´s take those called "AUTO", "MANUAL"... If we insert a text in Properties - User Defined 3 - Button Text, this text is shown in the Graphics Designer but not in Runtime. We tried changing language and several different things but it didn´t work...then we decided to insert a Static Text which meets more or less our requirements (that´s the way it´s working now) but it´s not the right solution cause it doesn´t let us press in the button itself but in the static text. Could you please tell me how could this be solved ? Could you please try to open it and see if texts can be seen in your PCs ?? - Another important fact related to this .pdl happens when we pressany button (AUTO f.i.) and keep the mouse clicked. In the moment we move the arrow out of the button and stop pressing it, the button keeps pressed, as if it were stucked. And what could be the reason for this ? If you have any doubt about my explanation, i can try to explain more clearly... ;) Any piece of advice is welcome ! And thank you very much in advance Ciao Attachment@PG_MBT2_STANDARD.zip (409 Downloads) |
6/7/2007 3:57 PM | |
Joined: 10/18/2006 Last visit: 7/29/2024 Posts: 163 Rating: (3) |
Ok, thanks a lot for your quick posts Ciao ! |
Follow us on