7/21/2014 7:46 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, There is a FAQ with a list of modules supported by TIA: http://support.automation.siemens.com/WW/view/en/50029532 If your modules are older than the configured modules, you risk to have "mismatch" errors. Because newer modules could have new features not supported by the older once. You will have an SF LED lit on the IM, and on the mismatching module. If your modules are better than the confifured modules, I do not expect that type of errors. |
Best regards |
|
7/22/2014 2:41 PM | |
Posts: 1368 Rating:
|
Hello Maxyx, you can try to import the GSD of ET200S into TIA Portal. I think, in this GSD the older modules are listed, too. http://support.automation.siemens.com/WW/view/de/19699080 |
7/22/2014 4:27 PM | |
Posts: 1058 Rating:
|
Hello Maxime, it is not a very safe procedure to use other GSD files as installed. There might be new features on newer modules, as well as older features might have been discarded. Why take the risk,when the GSD files you need are for sure available on internet, especially on siemens product page? regards |
Follow us on