10/13/2014 10:03 AM | |
Joined: 8/27/2010 Last visit: 6/3/2022 Posts: 417 Rating:
|
Hi! Here it is: 6ES7390-7BA00-0AA0 CheckSitopmanual for details, page 4/5. For other PS order number, please use same techniques) Keyword for search: PS-CPU connecting comb |
This contribution was helpful to
1 thankful Users |
10/13/2014 10:12 AM | |
Joined: 1/5/2011 Last visit: 4/6/2023 Posts: 814 Rating:
|
Thanks a lot olloy, are you sure I can use this one with my current set-up? What worries me is the description of this product:
The CPU314C PN/DP was released in 2011, will this work? Thanks in advance. Kind regards, Jens |
Keep it simple and on-topic. |
|
10/13/2014 10:30 AM | |
Joined: 1/21/2013 Last visit: 10/1/2023 Posts: 4617 Rating:
|
Hello Jens, mmmh alone? the connector comb is included with PS305/307 look at page 5/2 Catalog KT 10.1 · 2014 in the accessories does not say anything |
10/13/2014 10:46 AM | |
Joined: 1/5/2011 Last visit: 4/6/2023 Posts: 814 Rating:
|
Hi Ste39, yes I'd like to order them as spare parts, I know they come with the PS but they tend to get lost around here |
Keep it simple and on-topic. |
|
10/13/2014 11:04 AM | |
Joined: 8/27/2010 Last visit: 6/3/2022 Posts: 417 Rating:
|
I'm pretty sure it will fit. You cangooglethe image and check how it looks. Even if it will not fit, I think it cost couple of euros, so it will not be a problem to use a wire in this case. |
10/13/2014 11:24 AM | |
Joined: 1/5/2011 Last visit: 4/6/2023 Posts: 814 Rating:
|
thanks olloy, the thing is if I google it, this connector looks kind of flat, while the one I need bends a bit backwards, the PS contacts are located higher then the CPU contacts. This is the one matching the product code you've given me: http://i.ebayimg.com/t/Siemens-6ES7390-7BA00-0AA0-Verbindungskamm-/00/s/MzAwWDIyNQ==/$T2eC16d,!zQE9s3stYbcBQh6-ggWYQ~~60_35.JPG and attached is whatthe connector should actually look like. Can anyone help me further, maybe the Siemens experts?? Kind regards, Jens |
Last edited by: Jens_app at: 10/13/2014 11:25 AMKeep it simple and on-topic. |
|
Follow us on