10/3/2011 1:03 PM | |
Joined: 6/29/2006 Last visit: 9/4/2024 Posts: 53 Rating: (1) |
Hi All, I have several errors whilst trying to connect to a PROFINET IO-system, everything looks fine except for the errors. (By the way my device is a Cognex camera system) New I/O access error during process image update /n input? (? Bytes) will temporarily not be updated as part of the updating of process image 0 I thought I'd found the solution to my problems at /tf/WW/en/Posts/63081 I have installed Service pack 1 and just tried to install update 2 because it say's update1 is included in update 2 but it won't install because TIA is a newer version. I could try and download Update 1 but i suspect it also won't install for the same reason. I don't know what to do next? Many thanks in advance. *****EDIT***** Hmmm ok i'm a muppet, there is updates for non SP1 and SP1, as i installed SP1 first the non SP1 update does not apply. Hopefully my answer is in reach. |
Last edited by: Kev at: 10/3/2011 3:27 PMIt's only easy if you know the answer!!! |
|
10/4/2011 10:46 AM | |
Joined: 6/29/2006 Last visit: 9/4/2024 Posts: 53 Rating: (1) |
Thanks huggy_d1, I have to play a waiting game at my company because no one has admin rights to install software etc except I.T. but I will come back and let you know one way or the other.
|
It's only easy if you know the answer!!! |
|
10/11/2011 10:26 AM | |
Joined: 6/29/2006 Last visit: 9/4/2024 Posts: 53 Rating: (1) |
HI huggy_d1, According to the link below <quote> Integrated PROFINET Interface The new CPU-Firmware Version 2.0 of Simatic S7-1200 supports communication with Profi net IO devices as a Profi net IO controller. |
It's only easy if you know the answer!!! |
|
7/10/2012 5:25 PM | |
Posts: 3 Rating: (0) |
Hello I have the same problem trying to integrate a Cognex Camera to the s7-1200 by profinet. Does anyone know how to solve the problem??? Thanks
|
Follow us on