10/24/2017 9:38 AM | |
Joined: 11/29/2011 Last visit: 1/27/2023 Posts: 1346 Rating:
|
Hi, How do you do long-term archiving with WinCC flexible? How do you log tags and messages with WinCC Advanced V11 in an SQL database? Anyways if you have plans to expand, maybe should look at a S7-1500. |
- What you read here, please check with manuals and your requirements. |
|
This contribution was helpful to
1 thankful Users |
10/24/2017 10:28 AM | |
Posts: 86 Rating:
|
Hi MicroMan, Thanks for quick response. I have read the Long Term Data Archiving... i can see it's made on Wincc(PC) and Wincc flex(comfort), is it the same on the Basic panel as i mentioned i would like to use the 9" basic panel. The expand maybe on other site, and also currently the budget is low. also what about sending daily report to specified email address, can i make any datalogging temporary on the PLC? Any thought about the configuration, is there other way to to connect DP to PA networks(cheaper configuration)?
Thanks. |
10/25/2017 11:49 AM | |
Joined: 11/29/2011 Last visit: 1/27/2023 Posts: 1346 Rating:
|
Hi, You need a scriptable HMI with archiving capability. You can check on that in the Specification of the HMI( SIMATIC HMI HMI devices Basic Panels 2nd Generation ). You could also consider to use a webserver for storing your data on S7-1200. You can check on that option in the SIMATIC S7-1200 Easy Book . PA... You could consider using DP/PA Link instead of a coupler. See the How do you set up the DP/PA link and how do you configure the DP/PA link and DP/PA coupler? I hope I could help a bit. |
- What you read here, please check with manuals and your requirements. |
|
This contribution was helpful to
2 thankful Users |
10/26/2017 8:32 AM | |
Posts: 86 Rating:
|
Hello, Ok i made some research and looks like the basic panels wont support scripting. Also took a look at the comfort panels seems all of the support scripting and archiving, does it matter if the panel would be 9" or 12", according to the reuirments i described? I thought about the option of the webserver datalogging but the customer required that the log would sent by mail, is there a possability to log the data to DB for 24h with 10 minute interval for 18 floating points tags and then sending it by mail? What the benefits or differrnce of using DP/PA LINK instead of DP/PA COUPLER? I read about this 2 ways of making such configuration, but still tries to understand what prefered and what better? Thanks a lot,
|
10/26/2017 11:42 AM | |
Joined: 11/29/2011 Last visit: 1/27/2023 Posts: 1346 Rating:
|
Hi, I do not think the matter of the screen matter as much. Check the device specification if the device support the function you need to use. DB. You could consider to actually create a DB and fill it with data in FIFO style. You could consider using a script that send an Email from the HMI. See theSIMATIC HMI WinCC V12 Comfort Panels, Runtime Advanced - Advanced Configuration Options There will be a fair bit of development work. To check the DB sizes and how to write block to filll the DB see the Programming Guideline for S7-1200/1500 PA.... Well. I think you should raise this question the Communication/ Networks conference. It is a bit wide topic for here. I hope I could help. |
- What you read here, please check with manuals and your requirements. |
|
This contribution was helpful to
1 thankful Users |
Follow us on