8/10/2008 5:50 PM | |
Posts: 33 Rating:
|
Dear J_Bell, Can you give me more information about ABT? Where can I gain more detailed information about this active bus terminal? Thanks in advance! Norbert |
8/11/2008 6:30 AM | |
Joined: 9/27/2006 Last visit: 12/9/2023 Posts: 12190 Rating:
|
Hello Meritor; The active bus terminator (6ES7 972-0DA00-0AA0) description can be found on the Siemens Mall, for example here: There is also a 3-page section on the ABT in chapter 5 of the manual "Simatic Net Profibus Networks" (profn2_e.pdf). However, as suggested earlier, please look atthe physical setup of your bus, it is weird that you should have to use such a low speed for such a small length. Do you have any diagnostic information available on the diagnostic buffer of the CPU? Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 8/11/2008 6:32 AM |
|
Follow us on