8/4/2014 2:23 PM | |
Joined: 7/28/2009 Last visit: 5/10/2022 Posts: 90 Rating:
|
Hi All, I have a configuration as per the attachment. When I dowload the hw configuration i get the error as attached. I use a MPI adapter on the PG Port of my profibus connector on the PLC's DP Port. When i check on accessible devices i can get the profibus address of the CPU but not of the IM. One more thing is that when i connect the MPI cable on the PG Port of the Profibus connector on the IM the leds of the Adapter are all OFF. Is that possible that the IM could be faulty? or any other suggestions? AttachmentHW Config.zip (106 Downloads) |
Last edited by: Revathy at: 8/4/2014 2:34 PMCheers |
|
Follow us on