10/4/2011 3:46 PM | |
Joined: 9/27/2006 Last visit: 3/20/2025 Posts: 12344 Rating:
|
Hello Aymen; Your PLCs are already Profibus-DP masters in their own projects; since the integrated DP port of the PLCs can act as a master ora slave, but not both at the same time, you would have to either: -insert a CP 342-5 and configure it as a DP slave so the PLC can be connected to the new master PLC; -use a DP/DP coupler as a double-slavebetween the b=new master and each existing PLC (you would need one per connection. In any case, there would have to be configuration and programming changes to be done in each PLC participating in these exchanges. Have a look at these different FAQs that will guide you through your conceptual musings: Master-slave connection between two CPUs in different projects What master/slave communication options are available on PROFIBUS DP? Notes on linking a CP342-5 as DP slave to a DP master with STEP 7 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/4/2011 3:46 PM |
|
10/4/2011 5:21 PM | |
Posts: 4 Rating:
|
You can create S7 connection over Profibus and read from remote CPU any DB or M with SFB14 "GET". But problem: Itried,I made configuration, but Ican't use integrated interface.May be someone explain it.Iused Profibus CP. AttachmentTests7pb.zip (196 Downloads) |
10/6/2011 12:05 PM | |
Posts: 4 Rating:
|
I'm sorry I don't understand what do you mean aspire. |
10/6/2011 3:53 PM | |
Joined: 9/11/2011 Last visit: 9/10/2024 Posts: 53 Rating:
|
Here is the network that exists in one of six machines. The PC that I will use has a communication processor CP 5611 A2 PCI CARD. I have to use a new PLC in which I will programmed another function to calculate the uptime and downtime. Do I connect the new controller with all PLCs using the MPI network and connect the PC runtime with the new PLC using a PROFIBUS network? If I do this it is necessary to change all the PROFIBUS addresses of all PLCs that exists in each machine? Is it necessary to group all the project in one project, even it I will use the MPI network between PLCs? AttachmentIMAGE.zip (170 Downloads) |
Follow us on