5/30/2014 9:13 AM | |
Joined: 11/21/2007 Last visit: 3/31/2025 Posts: 2326 Rating:
|
To Select the Instruments Communication type you need to discuss the same with your Instrument supplier . Profibus networking is more prpular for interfacing Remote I/Os , Controllers , Drives etc with relatively large amount of data per device. Usually PA instruments are polular in process control applications where large no of field instruments are installed with small amount of data per device. Networking pf PA Devices is easier as bus splitters can be used. For more information regarding Profibus DP and PA pl see dchartier's post in the Thread : Profibus DP & PA
As he says : choose based on price, availability and usefulness Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to
1 thankful Users |
Follow us on