12/7/2016 9:04 AM | |
Posts: 1 Rating:
|
hello every one, i was writing a program to control a drive i.e danfoss fc300 with s7 300 ppo type 6 word consistent all the parameter setting and the configuration are ok bat as soon i put the drive in run mode i will have a profibus fault (w34) in the drive and plc also in profibus fault . the confusing part is if i increase the speed the drive speed also increase so u experts can you help me on that thnks ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/7/2016 9:56:01 AMNew subject after splitting |
|
Follow us on