7/9/2009 12:26 PM | |
Posts: 4 Rating: (0) |
Hi, Could you send me luist of the faults arisis in the profibus network and its expected reasons. |
7/9/2009 1:02 PM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242) |
Hello, I don't know what you really want, but you should check SFC51 in Step-7 online help system and look here also http://support.automation.siemens.com/WW/view/en/26996747 |
Best regards, |
|
7/9/2009 1:13 PM | |
Joined: 9/27/2006 Last visit: 5/2/2024 Posts: 12257 Rating: (2666) |
Hello Omarlara; This might not be exactly what you are asking for, but I use this document regurlarly to prepare commissioning teams who have to deal with installed Profibus networks (DP and PA). There are chapters on commissioning and troubleshooting techniques and instruments, butmore importantlysome checklists in the Appendix that you can use to ensure that the network cabling, connecting and terminationhave beendone properly. These are generally the sourceof almost all Profibus networkproblems I have run into. By the way, this document was located in the Profibus.com download pages; it saeems to have been updated, but I haven't checked out the new versions (these include Profinet installation and commissioning).But this version is still useful, and the information still holds up to the test of time and practicality.. Hope this helps, Daniel Chartier AttachmentGuideline_Commissioning_8032_v101_Feb06.pdf (98 Downloads) |
Last edited by: dchartier at: 7/9/2009 2:37 PMI have located the Profibus installation and commissioning guidelines on Profibus.com. Here is the link: http://www.profibus.com/index.php?id=12&no_cache=1&tx_pxdprofibus_pi2[download]=3&tx_pxdprofibus_pi2[mode]=display |
|
This contribution was helpful to2 thankful Users |
7/9/2009 1:29 PM | |
Posts: 4 Rating: (0) |
Thanks a lot |