11/17/2017 11:24 AM | |
Posts: 6 Rating:
|
Dear experts; I'm having trouble setting up the communication between my CP342-5 and the CP443-5 Basic of my customer. Originally, profibus was ordered for this project. For us, our standard is Profibus DP but on site I noticed this was not possible for the client so he wanted me to change to Profibus FDL. I've added the FDL connection (to unspecified partner) on my PB subnet and added all the necessary settings as PB address and LSAP. However; the communication is not working. My AG_SEND block status is alternating between 8181 and 8315. It seems that it goes in error (with status 8315) everytime it tries to send data. I've received some data from the customer but he also had a lot of error messages. When I looked at the buffer of my CP I noticed is was constantly entering and dropping out of the logical token ring, therefore not being able to send data. The weird thing about this is that I made a test-program were I configure a master to check my communication and this works perfectly fine. On site however, no communication is possible. The only difference with my master test-program is that I use a different CP because I don't have acces to a CP443-5. General set-up: Slave (me): PB address: 15 - LSAP 2 I have added some screenshots to make everything as clear as possible. Yesterday I spent a whole day trying to solve this, but no luck. I wonder what you guys might have as solution. Thanks in advance! RN AttachmentPictures.zip (62 Downloads) |
Follow us on