4/11/2017 12:24 PM | |
Joined: 9/18/2015 Last visit: 6/4/2024 Posts: 132 Rating:
|
i have make FMS PROFIBUS connection between two s7-300 plc via CP PROFIBUS all communication parameters are well it make me green led (connection ready to send variables)in netpro view,i have configured the commnication variables in server which they willbe converted by the CP to FMS structure ,this structure must read by the client via GetOD requet in order to have the symbolique name of communication variable when i put FB3 in the client program the parameter of the bloc VAR1 did not accept communication variable adresse knowing that this parameter point to the area of communication variables that must be read from serveur PLC what must i do to solve this situation? you find in the attached file screen shoot of different step of configuration and also for diagnostic NCM AttachmentFMS PROBLEME.zip (90 Downloads) |
4/12/2017 12:50 PM | |
Joined: 8/3/2009 Last visit: 3/14/2025 Posts: 14990 Rating:
|
Hello narove Im no specialist at this topic but perhaps the following FAQ helps: https://support.industry.siemens.com/cs/ww/en/view/20982954 look in the linked Manual at Chapter 40 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on