9/28/2017 5:01 PM | |
Posts: 3 Rating:
|
Dear Dchartier Thanks for the fast response! I pasted some pics of the config in a word doc. The trouble shoot i get on the Diagnostic Buffer Always points at an IO device error (from the intelligent slave). Maybe I have to declare the 314 as an IO device on profibus, but how? Even if I use a document for the configuration of an intelligent slave from Siemens he still gives an error. Today i also tested the MPI over the profibus network and the PC could read all the components with PG/PC interface. Tested the firmware also and is all oké. I think i'm missing something, probably something small... Any suggestions for a new set up are welcome. Attachmentfouten.docx (91 Downloads) |
Follow us on