10/13/2010 7:11 PM | |
Joined: 9/27/2006 Last visit: 3/22/2025 Posts: 12344 Rating:
|
Hello Juan; Another soultion would be Siemens' Amprolyzer, a Profibus monitoring software that runs under Windows XP, uses Excel to generate reports and trends, and requires a CP 5611 Profibus communication processor installed on the same computer as Amprolyzer. Amprolyzer description and requirements: Essential functions of Amprolyzer V3.2 § Message frame recording with trigger and filter options relating to events and message frame contents, including time stamp § Storing and exporting message frame recordings in Excel format § Lifelist with all stations on the PROFIBUS § Overview diagnostics with the current operating states of the nodes § Bus statistics with the number of events, e.g. timeouts or message frame repeats § Automatic detection of the transmission rate System requirements for Amprolyzer V3.2 § 10MB available hard disk memory § Microsoft Windows2000 (SP2 and higher) / Windows XPProfessional operating system (administrator rights required) § Microsoft Excel 2000/XP/2003 § CP5611 communication module (PCI) Note: SIMATIC Field PG, Power PG, PG720 and PG740 use the CP5611 as an integrated PROFIBUS interface The Amprolyzer does not require installation of STEP7. However, STEP7 and Amprolyzer can be installed on the same computer Free Download:http://support.automation.siemens.com/WW/view/en/18818699 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/13/2010 7:13 PM |
|
Follow us on