Industry Online Support
Technical Forum
4/11/2014 1:50 PM | |
Posts: 133 Rating:
|
Hello, I have configured a Profibus network containing 2 PLC (CPU 313C-2 DP) one as a master and one as a slave, and also an IM151-1 (for ET200S). I have two error messages concerning the two PLC: for each PLC, the message says that there is no logic adress master/slave. How can I fix that ? here is my configuration
AttachmentPATES.zip (86 Downloads) |
5/30/2014 9:32 PM | |
Joined: 10/19/2012 Last visit: 4/17/2022 Posts: 315 Rating:
|
Pls. see attached file.
AttachmentNew Microsoft PowerPoint Presentation.zip (90 Downloads) |
5/30/2014 10:43 PM | |
Joined: 7/2/2008 Last visit: 3/14/2023 Posts: 928 Rating:
|
Helloallayahassine, The problem is that you didn't configure the data you want to exchange between the 2 CPUs. In addition toSMHZ'sreply,you will find more detailed procedures in Do the same steps as if the your master CPU is the S7-400 CPU in the example. Best regards, H-H
|
Follow us on