9/23/2014 1:06 PM | |
Joined: 11/21/2007 Last visit: 3/16/2025 Posts: 2326 Rating:
|
Hello Jengeese
Usually this should be a IE/PB LINK and not a Scalance ...
If you open the hardware configuration, you will notice that besides the Profibus address ( 12 , 13 etc ) each drive also has a peripheral address area ( PIW / PQW ) assigned to it. What you are seeing in the program is the Peripheral address ( PIW / PQW ) : e.g. W#16#208 Hex = 520 Decimal .. i.e. this is referring to the drive with peripheral address starting with PIW / PQW 520 and so on. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to
1 thankful Users |
9/24/2014 8:43 AM | |
Posts: 84 Rating:
|
Thanks for explanation. Now it is clear for me.. |
This contribution was helpful to
1 thankful Users |
Follow us on