7/15/2013 11:23 AM | |
Posts: 47 Rating:
|
Hi, thanks for your reply.... Among Profibus PA and FFB, which should be used? |
7/15/2013 12:29 PM | |
Joined: 3/18/2008 Last visit: 8/25/2022 Posts: 1750 Rating:
|
PROFIBUS PA (Process Automation) is used to monitor measuring equipment via a process control system in process automation applications. This variant is designed for use in explosion/hazardous areas (Ex-zone 0 and 1). The Physical Layer (i.e. the cable) conforms to IEC 61158-2, which allows power to be delivered over the bus to field instruments, while limiting current flows so that explosive conditions are not created, even if a malfunction occurs. The number of devices attached to a PA segment is limited by this feature. PA has a data transmission rate of 31.25 kbit/s. However, PA uses the same protocol as DP, and can be linked to a DP network using a coupler device. The much faster DP acts as a backbone network for transmitting process signals to the controller. This means that DP and PA can work tightly together, especially in hybrid applications where process and factory automation networks operate side by side. Foundation Fieldbus is an all-digital, serial, two-way communications system that serves as the base-level network in a plant or factory automation environment. It is an open architecture, developed and administered by the Fieldbus Foundation. It's targeted for applications using basic and advanced regulatory control, and for much of the discrete control associated with those functions. Foundation fieldbus technology is mostly used in process industries, but nowadays it is being implemented in powerplants also. FOUNDATION fieldbus was originally intended as a replacement for the 4-20 mA standard, and today it coexists alongside other technologies such as Modbus, Profibus, and Industrial Ethernet. FOUNDATION fieldbus today enjoys a growing installed base in many heavy process applications such as refining, petrochemicals, power generation, and even food and beverage, pharmaceuticals, and nuclear applications. A typical fieldbus segment consists of the following components.
|
VANDE MATARAM..... |
|
This contribution was helpful to
1 thankful Users |
Follow us on