12/31/2012 2:25 PM | |
Joined: 4/22/2010 Last visit: 12/15/2022 Posts: 5697 Rating:
|
Hello, Only thing you can do is deactivate the DP station before turning it off. For more information System Software for S7-300/400 System and Standard Functions Chapter 16 descibes the function SFC 12 "D_ACT_DP" |
Problem solved? |
|
12/31/2012 4:27 PM | |
Joined: 3/21/2006 Last visit: 4/12/2023 Posts: 10221 Rating:
|
If the CPU doesn't go in STOP(http://support.automation.siemens.com/WW/view/en/19350076) mode would not a be problem. The correct way isMarcjansuggestion. Best regards, Hristo Mihalev
|
1/1/2013 9:53 AM | |
Joined: 3/21/2006 Last visit: 4/12/2023 Posts: 10221 Rating:
|
Give us details about network baud rate and distances between each nodes. |
1/2/2013 6:45 AM | |
Posts: 21 Rating:
|
hello sir here is my attechment of diagnotic detail. working baud rate 1.5 mbps and distance between each node is .5 meter or less than .nodes are comming temprary .than gose out ..
Attachmentdiagnostic detail.one.pdf (77 Downloads) |
Follow us on