6/1/2011 7:45 PM | |
Posts: 8946 Rating: (999) |
Did you restart DP-Master? (Power off/on at CPU) |
This contribution was helpful to2 thankful Users |
6/1/2011 7:48 PM | |
Posts: 109 Rating: (11) |
I cant.. Because My system is running and I can not risk of restarting.. I asked my boss but I am not allowed.. |
6/1/2011 7:50 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477)
|
Well Green LED flashing means, there is No Problem in communication but Your PLC sends some unusual datas or drives can not read it properly.. Normally, I am agree with IBN-Service that you have to re start your DP-Master.. PLC Regards, Devesh |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to1 thankful Users |
6/1/2011 7:52 PM | |
Posts: 109 Rating: (11) |
Thank you both for your Quick replies.. |
6/8/2011 8:48 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Take a look there Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails? best regards, Hristo Mihalev |
Follow us on