Industry Online Support
Technical Forum
8/18/2009 5:47 PM | |
Posts: 33 Rating:
|
What are the differences between and similarities between Profibus and Profisafe? Regards, Mike |
8/19/2009 3:40 AM | |
Joined: 10/7/2005 Last visit: 2/14/2025 Posts: 3036 Rating:
|
Hello Mike All that PROFIsafe reallymeans it toembedd (add) a(safety related/required) message inside the "normal" Profibus DP message (or Profinet for that matter) to achieve SIL3/CAT4 rating of the communication. Exactly how this is done is best explained in the"Profisafe system decription" pdf which is availbale as a a free downloadfrom http://www.profibus.com/,the direct link to the download pageis: Profisafe system decription I hope this helps |
Last edited by: fritz at: 8/19/2009 3:46 AMCheers |
|
This contribution was helpful to
2 thankful Users |
Follow us on